What are the RS-485 parameters used for Infinet communications?

Issue

What are the RS-485 parameters used for Infinet communications? The baud rate can be set but the other parameters are not exposed in the Comm Port settings.

Product Line

Andover Continuum

Environment

Continuum Infinet

Cause

Values not exposed in Comm Port settings dialog.

Resolution

The Infinet Protocol RS-485 parameters used:
 
1 start bit
8 data bits
No parity
1 stop bit
No flow control