Cannot save WorkPlace Tech Tool Editor application file for MNL-800 controller

Issue

After editing a MNL-800 application with the WorkPlace Tech Tool Editor, an error is displayed indicating that the application file could not be saved.

Product Line

SmartStruxure Solution

Environment

SBO 1.4, 1.4.1 or 1.5

Cause

The name of a LON Network Variable (nvi or nvo SNVT) or a LON controller configuration constant (nci SNVT) contains a space.

Echelon standards do not allow spaces in network variable or configuration constant names.

Resolution

Edit the application file removing any spaces or other non-supported characters from network variable and configuration constant names.

More information is contained in the SBO WebHelp topic "WorkPlace Tech Editor"