Display Window in AMT for all open Windows in I/NET

Issue

Display Window in AMT for all open Windows in I/NET

Product Line

TAC I/NET

Environment

INET site

Cause

In AMT, how does one see all the open windows that I/NET has open?

Resolution

In AMT, there is a new Window in the Task Bar which allows the user to see all the open windows that I/NET has open. This includes Alarms, Messages, Transactions, Graphics and Tools.

To use this, the following steps should be followed:

  1. Open AMT, on the task bar to the far right next to the "?" there is an Icon that looks like a window.
  2. Click on it and it opens an Editor that lists all the windows that I/NET currently has opened.
  3. The user can choose whether they want to close a window or leave it open based on the amount of information he wants to see on his screen.

Note: Having multiple windows of the same information (AMT) may cause AMT to lock up and or shut down.