Filtering Alarms in StruxureWare Building Operation to show only I/NET alarms

Issue

Filtering Alarms in StruxureWare Building Operation to show only I/NET alarms

Product Line

TAC I/NET, SmartStruxure Solution

Environment

I/NET integrated to StruxureWare Building Operation

Cause

Users may wish to only view alarms from the I/NET system

Resolution

Filter for All I/NET Alarms:
 
  1. Create an alarm View
  2. Click on the Filter Object
  3. Add a condition to Filter by Type
  4. Select the Type 'INET Alarm Record'
  5. Click OK

 

Filter for I/NET Alarms from a Specific Link

 

  1. Create an alarm View
  2. Click on the Filter Object
  3. Add a condition to Filter by Source
  4. Type */INET Interface/LL where LL is the link number of the desired link. NOTE: if the INET interface on your server is not the default name, the name must match yours exactly.
  5. Click OK