Issue
In Continuum the process of disseminating the communication settings (IP address etc) of a controller/Cyberstation to all the peer controllers on the network is accomplished via the 'TEACH' functionality.
What is the equivalent of the 'Teach' in StruxureWare Building Operation?
Product Line
SmartStruxure Solution
Environment
Enterprise Server
Automation Server
AS
ES
Cause
Documentation
Resolution
In StruxureWare Building Operation similar functionality is accomplished via the ES's 'Repair server communication' feature
Right click on the ES and select 'Advanced->Repair server communication