Settings are not the same when TAC Vista is running as a Service

Issue

Why do we get different settings when TAC Vista is running as a Service compare to started normally.

Product Line

TAC Vista

Environment

TAC Vista

Cause

When TAC Vista is running as a Service, it is using "System user", and not the same user that is logged in.

Resolution

Verify that the system user have correct settings to be able to run TAC Vista as a Service.

Under Region and Language, under the tab Administrative, you find Current language for non-Unicode programs, and also a button named Change system locale...