Object type mismatch error when reloading inputs or output to a b3 Controller

Issue

During reloading of controller when physical points are reloaded a Object Type Mismatch error occurs.

 

Product Line

Andover Continuum

Environment

  • b3
  • Reload

Cause

Controller database issue.

Resolution

In this case the problem was resolved by...

  • Deleting the bacnet instance of the controller.
  • Deleting the Infinity instance of the controller in offline mode.
  • Relearning the controller.
  • Rebuilding the controller configuration manually.
  • Finding the bacnet device and sending to database.