Is there a demo license available for the Continuum OPC Server?

Issue

Requirement for a demonstration license for the OPC Server to get an idea about how it functions and to demonstrate to potential customers.

Product Line

Andover Continuum

Environment

Continuum OPC Server

Cause

Require demonstration license for the software.

Resolution

There is a one hour demonstration mode that the software goes into if there is no valid license found. This should provide enough time for demonstration purposes.

When starting the application without a valid license the below dialog is displayed.

 

You can download the Continuum Controller OPC Server from the downloads website at this link.