Do the old Belimo Bacnet b3865 VAV controllers work when transitioning to an Automation Server?

Issue

Transitioning from Continuum to Struxureware Building Operation and replacing bCX's with Automation Servers.
 

Product Line

Andover Continuum, SmartStruxure Solution

Environment

b3865

Struxureware Building Operation

Cause

Unsure if the older belimo style VAV controllers are compatible with StruxureWare Building Operation.

Resolution

All of the b3xxx controllers (including both the -V and non -V) will work with the Automation Server under it's MSTP network.

Also check out the b3 VAV Quick Start Video on the Exchange.