IP rating on SE7000/SE8000

Issue

It is required to know the IP rating on the SE7000 and SE8000 range devices, but this is not written in the datasheet.

Product Line

SmartStruxure Lite

Environment

SE7000
SE8000

Cause

The information was not available at the time where the datasheets were created.

Resolution

The IP rating on the devices is IP30. At the time of writing, tests are ongoing for IP31 rating.