Can past exception events be cleared from b3 Schedules?


A Schedule in a b3 under an Automation Server does not seem to have the same option to clear events that the Automation Server has or that was present when the same b3 is under a bCX in Continuum.

Product Line

SmartStruxure Solution


Automation Server

b3 controllers


There is no option to delete multiple exception events from b3 Schedules similar to what can be done in the Automation Server.


 They will need to be removed individually or wait until the exception event expires which should them remove them from the Schedule.