Schlage Integration with PIN

Issue

Using PIN only for the Integration and it is not working.

Product Line

Andover Continuum

Environment

Continuum Version 1.94 and above.

Cause

The X Driver has a limitation on how it functions with PIN only.

Resolution

To resolve this issue, DO NOT use PIN only as it is not supported by the X-Driver. If the PIN needs to be used then it must be Card and PIN.