Is there any way to mass change any of the bCX / ACX / NC2 settings as configured from the controllers configuration webpage?

Issue

Is there any way to mass change any of the bCX / ACX / NC2 settings as configured from the controllers configuration webpage? 

Product Line

Andover Continuum

Environment

ACX57x0

CX9680

bCX9640

bCX4040

CX9702

Cause

Settings need to be changed en-mass for a large number of Controllers. In one particular case there were a large number of ACX57xx’s that needed to have the first and second SNMP alarm target PC's IP addresses changed for all controllers.

Resolution

There is no way to set all of these at once. As with all of the settings on the controller configuration webpage, they will need to be manually changed one at a time by connecting to each individual controllers configuration webpage.