Issue
Connecting to Controllers using Dial.
Environment
I/NET Seven Site
Cause
How to connect to remote sites using Integrated Dial
Resolution
If the user is connecting to remote sites using Integrated Dial and the site controllers are not visible, please check the following settings:
- Open I/O Server, modify the dial profile
- Uncheck the Dial Box
- Shut down and restart I/O server
- Connect again
If the user is connecting to remote sites using ADAA and the site controllers are not visible, check the following setting:
1.DTE (Host)--------DCE (Modem)-------DTE (Controller)-----9600 (Baud)
All these need to be at 9600 Baud, otherwise the lights on the I/O Server would only show Red and no Green. This indicates that there is a Transmit but no receive between one of the above components. For I/NET Seven, only the US Robotics 56K Modems are supported.