Adding IO Software Points to an AS-B

Issue

User unable to find means to add I/O points for an AS-B in workstation

Product Line

SmartStruxure Solution

Environment

Automation Server Basic

Cause

User not selecing the AS-B-XX onboard IO object

Resolution

  1. In the system tree browse to the IO Bus/AS-B-XX onboard IO
  2. Right click on the object and select New/Input or Output Point
  3. Select the type of IO and continue creating the IO point.