Issue
Unable to create/edit Reports or Schedules with Windows Authentication enabled on the Workstation.
1. All fields greyed out when attempting to edit a Report object
2. See a "Security error: Security logon rejected" error when attempting to create a new Schedule object.
Environment
Continuum v1.94
Continuum v2.0
Cause
With Windows Authentication enabled, Continuum user credentials were being used for certain internal processes to effectively login to Windows. Since the credentials may not match the authentication would fail.
This has been corrected with Continuum v2.0 SP1
Resolution
The issue has been resolved in Continuum v2.0 SP1. Download Continuum v2.0 SP1 installation files from here.