Report object setup to output to directory doesn't save to multiple files.

Issue

Report setup to automatically save to unique files in an output directory is not working. When ReportCmdLine.exe is used to save the report output (see  Article #6528) only a single file is created and overwritten each time.

Product Line

Andover Continuum

Environment

Continuum Cyberstation

Continuum Report object

Cause

The name of the Report object being run has a period (.) in its name.

Resolution

Rename the Report object removing the period from its name. The Report output will now save a new file with date and time in the filename each time it is run.