Error importing a StruxureWare Building Operation export file

Issue

Error importing a StruxureWare Building Operation export file. Below is an example of the error. 

ERROR: Import failed to commit changeset transaction with an exception. RecoverableException: /home/ci/ci-build/rb-rb-1.8.1-system/source/server/nsp_servers/csc/changesetmanager/source/ChangeSetTransaction.cpp(1442) Invalid Data Error: File_Extension_Not_Permitted (0x10048) in module Security_Manager(74). "Not permitted to store the file "htgseqintro.wmv" with the current Document Policy." - Stack

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation 1.8

Cause

The export file contains a document file extension that is not permitted in the Document Policy Permitted File Extensions

Resolution

The file extension has to be added to the Permitted File Extensions list. See Adding a File Extension to the Permitted File Extensions List on Web Help.

For the error example shown in the issue of this article, the extension wmv has to be added to the Document Policy Permitted File Extensions. list.