Creating Access Levels

Issue

How to create an Access Level

Product Line

AccessXpert

Environment

AccessXpert

Windows Server 2012 and Above

Cause

How to create a new Access Level

Resolution

To create a new Access Level in AccessXpert, the following steps needs to be followed:

1. Select Access Configuration from the main headers, Add New Access Level

2. Name accordingly (7 X 7, Cleaners etc)

3. Assign Access Control Entry (drag and drop users from user list)

4. Use existing schedule or create a new one if needed

5. Use door group that has access to requested area or create accordingly

6. Click on Save