Creating a Door for Read In/Out

Issue

How to set up a Door on a controller for use as Read In/Out Access

Product Line

AccessXpert

Environment

AccessXpert

Windows 7

Server2012 R2

Server 2014

Cause

There is no documentation on how to do this in AccessXpert

Resolution

In order to do this, the following steps need to be followed:

1. Open up the site instance from IE

2. Log on to the system and Select the View All Hardware Icon

3. Select  the Interface that the door will be configured on

4. Check the box  for Card In/ Free Out on Door Behavior

5. Save and close

6. Restart the controller