Issue
Mag stripe on Badge will not encode after upgrading Windows and Cyberstation
Product Line
Andover Continuum
Environment
Windows7
Cyberstation
Fargo Printer
Cause
Badge printers use different printer drivers and configurations that can cause features to not work from one version of Windows and Cyber
Resolution
EpiBuilder>Tools>Printer Card Encoder Setup
Magstripe tab> Current Magstripe Encoder - Custom selected and working on the older printer, but not on the newer printer
Changed the selection to Fargo and now the encoding is working on the new printer (See image below)