Accessxpert Device Administrator

Issue

Where to go and download the application

Product Line

AccessXpert

Environment

Server 2012

SQL 2012 and above

Premise Install V2

Hosted V2

Applet V3

Cause

There is no doumentation on where to go to download the Device Administrator and how to program the SSC to communicate with the selected application.

Resolution

The following steps describe where to go and donwload the software and how to use it to program an SSC:

1. Open up an IE Browser and go to the url listed

2. In the search field type Device Administrator

3. Select the Accessxpert Device Administrator and download to any location

4. Browse to location and doouble click execute to run and install the program

5. Accept Agreement and click next to contnue installation

6. Click Next to start installing the software

7. Select location to where the file will be installed

8. Successfully loaded software 

9. Complete installation click on Finish

10. Connect the device to switch that is open to the Internet and Launch the application by Opening All Programs

11. Launch the application 

12. RIght Click on the usb line or click on the Green Arrow to the top left to upgrade the software

13. Once Upgraded successfully, Right Click again on the line and Select Properties then select the Ethernet 1 ConfigurationTab

14. Select applicable choice whether it is DHCP or Static addressing being used and click on OK.

15. Once the deivce comes back Online, select the DIP Switches Tab and check the box for Default User

17. Using the IP address given from step number 13, open up IE and browse to that address

18. Once opened configure the SSC per LL# 19092 http://buildingskb.schneider-electric.com/view.php?AID=19092