Alarm Control Panel - Number of entries for Cause Note, Action Note and Checklist

Issue

Alarm Control Panel - Number of entries for Cause Note, Action Note and Checklist 

Product Line

SmartStruxure Solution

Environment

SnartStruxure Building Operation Workstation 1.9

Cause

The maximum number of entries that can be added for Cause Note, Action Note and Checklist are not indicated in available documentation. 

Resolution

There are no hard coded limits to the number of entries that can be added for the Cause Note, Action Note and Checklist