Visitor Management in V3

Issue

How does Visitor Management work in V3

Product Line

AccessXpert

Environment

Accessxpert

Hosted

Premise

Version 3

Cause

No directions on how to confgure Visitor Management in V3

Resolution

In order to use Visitor Management in V3, here are the steps to get it configured:

1. Open up a Chrome brower and enter this url http://ax.accessxpert.com

2. Once the site comes up, enter the instance name and necessary user credentials 

3. From the AX Header,  Select Visitor Management Tab

4. Select the Kiosk Tab and Enter the visitor's name and email address and click Next to proceed

5. Enter the person who the Visitor is seeing, system will automatically pull up the person, click on Next

6. Capture the Photo of the Visitor and Crop accordingly

7. Sign into the Window and click on Check in to see "Person"

8. An email will be generated to that person to let them know that they have a Visitor

9. A badge will be shown on the screen which has the Visitor's Photos and information

10. Click on the Print Button to Print a badge that can be displayed on the Visitors body

11. Depending on the printer (eg. Dymo being used), there are some settings that may need to be set for a good picture to be captured and Printed

12. Choose the right paper source as well as scaling value.  In this case, it is set to 70

13. Once everything is correct click on the Print button to send to the respective Printer

14. Attach to the Visitor for duration of the Visit

15. Upon completion of the Visit, select Check Out and this will Check the Vistor Out of the system