No stencils in VisiSat software for the new MicroNet 50 series range

Issue

No stencils in VisiSat software for the new MicroNet 50 series range

Product Line

Satchwell MicroNet

Environment

  • MicroNet 50 series range
  • VisiSat

Cause

An upgrade is required to receive these stencils.

Resolution

  1. Go to the help menu, and select about VisiSat.
  2. If you are running VisiSat 2.0 then you need to request the latest version of VisiSat 2.1. VisiSat 2.0 to VisiSat 2.1 is a free upgrade
  3. If you are using VisiSat 1.1 or VisiSat 1.2, then you will need to purchase VisiSat 2.1.