Inovonics Wireless Interface problem

Issue

Inovonics Wireless Interface problem

Product Line

TAC Vista, Andover Continuum, Other

Environment

FA7403

Cause

Inovonics provides an interface to access wireless temperature sensors. The FA7403 receiver can be used to interface with Xenta equipment or Continuum equipment, however these interfaces use different protocols.

Resolution

The Xenta equipment requires a hexadecimal protocol which corresponds to the FA7403 receiver.

The Continuum equipment requires an ASCII protocol which corresponds to the FA7403-ASC receiver.

If you have the wrong receiver for the equipment you are trying to interface with then contact the Product Support Group for steps to reconfigure this device.