Issue
How does the "Door Closed Timer" work in the I/NET Seven Door editor?
Environment
I/NET site with Access Control
Cause
Explaining the Door Closed Timer in the I/NET Seven Door editor
Resolution
Set the duration of the Door closed timer to a value from 0 to 25.5 seconds (0.1-second increments).
This timer determines how long the door must remain closed (as sensed by the door sense switch) before an unauthorized door open condition will trigger a "forced door" message.
Use this feature to help prevent false "forced door" messages that can sometimes occur when a door closes, but then bounces enough distance to trigger a temporary open condition at the door sense switch.