Issue
There are some rules using the I/NET Seven "Working Offline" options.
Environment
I/NET site
Cause
I/NET Seven "Working Offline" options
Resolution
If you take a DCUxxxx.sav file from an older version of I/NET Seven and open it up thru the "Work Offline" in a newer version of I/NET Seven (Rev 2.xx) and modify that save file.
You will have issues with this DCUxxx.sav file, for instance if you return this modified DCUxxxx.sav file back in the older version of I/NET Seven you will see changes in the Time Schedules and "Door ATS" time schedules in a Mipped 7920 board.
It adds two new lines in Time Schedules and the "Door ATS". Here is what you will see in the "Door ATS"
- APB (Anti Passback) settings for that door.
- APB Reset for that door.
- This is the Original ATS Schedule.
So the Rule to follow is this:
If you are working with DCUxxxx.sav from I/NET Seven rev 1.xx, then you must use the same version of :Work Offline.
If you are working with DCUxxxx.sav from an I/NET Seven rev 2.xx, you must the 2.xx version of "Work Offline"