Issue
A Xenta 5/7/9xx used as a LON node is not showing data from Xenta programmable controllers, but the values are working in Vista and LonMaker. SNVTs from ASCs are showing up correctly in the Xenta 5/7/9xx.
Product Line
TAC Vista
Environment
- LonMaker 3.1
- XBuilder 1.6
- Xenta Server
- Xenta 511, 527, 701, 711, 721, 731, 913
- Xenta programmable controllers
- Xenta 280, 281, 282, 283, 300, 301, 302, 401, 401:B
Cause
If the LNS database that is browsed into the XBuilder project has programmable controllers with spaces in the names, they will not show data properly.
Resolution
-
Go back into LonMaker and rename all programmable controllers that have a space in the name.
Example: Use an underscore in place of every space. - Update the Vista database
- Reimport the LNS database into XBuilder
- Download the Xenta 5/7/9xx