How can the resource count be found for a Niagara R2 station?

Issue

How can the resource count be found for a Niagara R2 station?

Product Line

TAC I/A Series

Environment

Niagara R2 station

Cause

User can't locate the Resource counts using Workplace Pro or a web browser.

Resolution

There are two methods.

Using Workplace Pro,

  1. Open a station (Note:  the station must be running) 
  2. Highlight the station name
  3. Select Search > Resource Count in the drop-down menu bar (alt-R shortcut)

Using a web browser,

  1. In the address bar, type http://[stationHost]/prism/resources.
  2. Sign into the station using an Admin user account.
  3. This will display a summary at any level of the database. For each level there is a "Total objects" listing at the top of the page. This is where the resource count is displayed for that level.