Issue
Using Roam IO/2 through bluetooth on a PDA
Environment
- Roam IO/2
- PDA
Cause
Using the wrong comm port is a common issue after pairing up your Roam IO/2 with your bluetooth connection.
Resolution
Using Roam IO/2 through bluetooth on a PDA
Once the pairing of the devices is complete as laid out in the instructions of either the infinet or Bacnet Service tool users guide. You'll notice that bluetooth device manager editors differ from vendor to vendor, but basically all have the same functionality. The PDAs will assign two comm ports for each bluetooth device. One for outgoing and one for incoming comm ports. When setting the comm port in the tools/preferences through the Roam IO/2 PPC software, you'll need to set it to the outgoing port that the bluetooth devices manager assigns.