What is the easiest way to tell if a point is being exported due to alarm attachments or programs?

Issue

What is the easiest way to tell if a point is being exported due to alarm attachments or programs?

Product Line

Andover Continuum

Environment

Listview

Cause

Run a quick report on which points are exporting data outside of the system.

Resolution

The easiest method to determine what points are exported is to run a listview of points and have the column "Export" in the listview. Every point that is being exported will have a "True" in the export column.