Issue
What is the earliest revision of Niagara R2 that the ProView LON Display, jar files and software wizard will function with properly?
Environment
- Niagara R2
- ProView LON Display
- lonWorks jar file
- Distech wizard
Cause
Using Niagara R2 revisions outside of R2.301.428 through R2.301.529 will not function with the UNC and Distech wizard.
Resolution
The UNC and Distech wizard will function with Niagara R2 revisions R2.301.428 through R2.301.529.
The required files are available from The Exchange Extranet.
Run the provided executable. Then edit file names in the emb, nt, and nre/modules folders.
Keep the newest Distech files and the latest lonWorks jar file.