Issue
What's the best way to uninstall SIGNAL software?
Environment
SIGNAL software
Cause
Remove SIGNAL software from a computer that no longer need the software.
Resolution
Steps:
- Perform two backups - one with executables and one without executables. The backup with executables can be used to restore the entire SIGNAL installation if that is required. The backup without executables is good to have if SIGNAL is already installed on a computer and only job-specific files are restored
- In Windows Explorer, delete the SIGNAL folder and two files in the C:\WINDOWS directory: signal.ini & bit.ini
- Remove any shortcuts created on the desktop and in the Windows startup folder.
- Reboot the computer.