Issue
Intrinsic Alarms - (InfinetStatus & IOModuleStatus)
What are they and How do they work
Environment
Continuum workstation
Cause
Information on Intrinsic alarms feature.
Resolution
Intrinsic alarms are built-in alarms on each Continuum workstation. The event notifications for these alarms are located under the templates directory in the Continuum Explorer. The event notifications for these intrinsic alarms will need to have recipients added to them and configured in order to deliver alarms to a workstation. These 2 intrinsic alarms function the same as regular alarms since it's the Netcontroller delivering the alarm. Meaning that they do not need to have a recipient in the eventnotification setup to LOG the alarm in order for it to be entered into the database.