Issue
UltiVist/DMS, how to remove all or parts of the E: Segment.
Environment
UltiVist/DMS
Cause
Delete the E: segment database using KILBRNCH.
Resolution
KILBRNCH is a powerful tool, before doing the following procedure, BACKUP THE DATABASE.
In an OS/2 window, go to the FI directory and type SET NOFCS=TRUE (this command turns off communications so that the KILBRNCH command will delete only the elements in the UltiVist database set to 'offline'). Press Return.
After getting x:\FI prompt back, type KILBRNCH FI (example KILBRNCH \FI\FI E:001.12.01.023).
This will delete (or kill) the database from that branch.
- E: is the Segment
- 001 is the Network ID
- 12 is the Panel ID
- 01 is the DCM ID
- 023 is the Controller ID
After completion, go to FI directory and then type SET NOFCS=FALSE.
Refresh the E: Segment.