There is a possible corruption of the SQL Database and the DCUxxxx.sav files when upgrading I/NET Seven from Rev 1.xx to I/NET Seven rev 2.13 and above

Issue

There is a possible corruption of the SQL Database and the DCUxxxx.sav files when upgrading I/NET Seven from Rev 1.xx to I/NET Seven rev 2.13 and above

Product Line

TAC I/NET

Environment

I/NET site 1.xx

Cause

corruption of the SQL Database and the DCUxxxx.sav files

Resolution

The Work-around is described in that attached document.

Possible Corruption when doing