Issue
Webpinpoint gives error, Could not connect to server. Cause:Type missing for member of type Object_ContectID
Environment
Webpinpoint graphics for webclient
.NET Framework 1.1
Cause
Hotfix issued by Microsoft (KB928366) was installed.
Resolution
This issue happens on webpinpoint graphics for webclient installations using .NET Framework 1.1, versions 1.6x through 1.73.
A hotfix was issued by Microsoft that caused this issue KB928366.
The solution is to remove KB928366 or upgrade to a version of webclient that uses .NET Framework 2.0, versions 1.74 or greater.