Registration of TAC Vista OPC server as service fails

Issue

Registration of TAC Vista OPC server as service fails

Product Line

TAC Vista

Environment

OPC Server

Cause

During the installation of TAC Vista OPC server, it might fail to register as a Windows server if you do not have a valid license for the TAC Vista OPC server during the installation phase. 

Resolution

  1. Uninstall the OPC Server
  2. Make sure you have a valid license
  3. Reinstall the OPC Server