Issue
Alarms in Menta not coming into Vista if the output is connected to additional logic.
Environment
Menta IV
Vista IV Workstation
Alarm Queue
Cause
Many times Alarms will be used to start backup systems in the event of equipment failure. This is commonly performed by attaching the output of an alarm to additional logic which will route needed information to the backup system.
Resolution
Add a DELB (binary delay) to the output of the alarm before connecting the additional logic. This will allow the alarm to show up in Vista Workstation.