Issue
When using "link builder" in WorkPlace Commissioning Tool, MNB-V2s and MNB-300s link OK but links to MNB-1000s do not work.
Product Line
TAC IA Series
Environment
- WorkPlace Commissioning Tool
- I/A Series MNB VAV
- I/A Series MNB 70
- I/A Series MNB 300
- I/A Series MNB 1000
Cause
An incorrect value set for APDU retries in the MNB-1000.
Resolution
- Use WorkPlace Commissioning Tool to display the devices, and double click the MNB-1000 in question to display the Device Properties window.
- Select the Advanced tab and ensure APDU retries is not set to 0. If it is, set it to 3, reboot the controller and the links will function properly.