MN50 Controller Optimisers Run-up/down influence node error.

Issue

Is there a fix for MN50 Controller Optimisers and the Run-up/down influence node error. PIB 07.11.02-1

Product Line

Satchwell MicroNet

Environment

  • MN50
  • PIB 07.11.02-1

Cause

A firmware upgrade is required.

Resolution

Version 5.02 Firmware now fixes this problem.