Issue
New MNET-CI and MNET- Air Balance software for MicroNet 2000 controllers is compatible with Windows XP and Vista.
Environment
MicroNet 2000 software; MNET-CI and MNET- Air Balance, Version 4.0
Cause
Release of software MicroNet 2000 software; MNET-CI and MNET- Air Balance, Version 4.0
Resolution
New versions of MNET-CI and MNET- Air Balance software for MicroNet 2000 controllers are compatible with Windows XP and Vista. The software is bundled with the 6 PSI tools in a zip file, PSIv4.1.zip. The zip file includes an installer and a READ.ME file that includes Release Notes and Installation Instructions.
The same converter, MN-CIM, that works with existing version of MNET-CI and MNET-Air Balance, will also work with the new version.
(NOTE: MN-CIM is obsolete as of December, 2011. See Product Announcement PA-000164. There is no functional replacement available)