Issue
A new BACnet jar file is available for Niagara R2 UNCs - bacnet-2.305.527i.v1.jar is available on The Exchange Download Center
Environment
- Niagara R2 UNC
- bacnet-2.305.527i.v1.jar
Cause
Information about the new BACnet jar file
Resolution
A new BACnet jar file is available for Niagara R2 UNCs - bacnet-2.305.527i.v1.jar can be downloaded from The Exchange Download Center.
The zip file contains a READ_ME_FIRST document that provides installation instructions, as well as a BACnet.Properties file to be installed in the UNC. The new jar file will improve the reliability of polling for BACnet data.