Issue
Can Niagara R2 / G3 operate on Windows XP Service Pack 3?
Environment
Niagara R2 / G3
Cause
Windows XP SP3 is not an approved platform for the IA Series.
Resolution
The recommendation at this time is to remain with Windows XP Service Pack 2.
For more details, read TPA-RKFD-08-0008.01 "Windows XP SP3" on the ExchangeOnline web site.