Issue
Are all four RS-485 ports licensed for use with BACnet/MSTP on a Niagara G3 ENC-520?
Environment
Niagara G3 ENC-520
Cause
Licensing information about the Niagara G3 will help during installation.
Resolution
Yes. At any time, any of the four RS-485 ports can be used without the need for re-licensing.