Issue
When using a Niagara R2 Master Enterprise Server, do the projects require the same Project ID?
Environment
Niagara R2 Master Enterprise Server
Cause
Project ID is required for license information.
Resolution
Example: Two projects will eventually have a Master Enterprise Server (MES) over both of them. One of the projects is in progress and the second phase will follow. In order to use a MES and allow both projects to communicate with it, do both projects need to have the same Project ID? Or can each separate Enterprise Server maintain its own Project ID?
Requirement: The MES is licensed to support multiple Enterprise Servers (with different project IDs). Purchase the IA-MES-1 which supports an Enterprise Server for one site. Additionally, each IA-MES-N would add another Enterprise Server (additional site). The project IDs for each Enterprise Server site would have to be provided in the license request form. The license will then list multiple project IDs and add the multisite feature.