Issues with some portions of Vista 5.1 on Microsoft Windows Vista

Issue

Issues with some portions of Vista 5.1 on Microsoft Windows Vista

Product Line

TAC Vista

Environment

  • Microsoft Windows Vista
  • TAC ToolPack
  • TAC Signature
  • TAC Webstation
  • TAC OPC Server for Danduc

Cause

Not all portions of Vista 5.1 are supported on Microsoft Windows Vista.

Resolution

While TAC Vista supports Windows Vista in release 5.1.0 the following programs are not supported:

  • TAC Toolpack
  • TAC Signature
  • TAC Webstation
  • TAC OPC Server for Danduc

Note: This is still true for version 5.1.1 despite this only being stated in the Vista 5.1.0 release notice.