Issue
Having issues accessing a remote BACnet network on a Niagara R2 UNC.
Environment
- Niagara R2 UNC
- BACnet network
Cause
Configure the Niagara R2 UNC as a BBMD device.
Resolution
When attempting to access a remote BACnet network from a computer over the Internet, the Niagara R2 UNC on the network must be set up as a BBMD device. Then, in the Commissioning Tool, configure communications so that the computer is accessing the remote network, using the IP address of the UNC set up as a BBMD.