Issue
The Niagara G3 Microsmart Driver Installation and Configuration Guide (F-27523) lists "Applicable Documentation" on page iv. Is that documentation available for download?
Environment
Niagara G3 MicroSmart Drive (Installation and Configuration Guide)
Cause
Manuals (F-25695, SOFT-MCN-101) are not available.
Resolution
Two documents in the list are obsolete and were inadvertently listed as available. They are:
- DCT MicroSmart Reference Manual (F-25695)
- MicroSmart Application Manual (SOFT-MCN-101).
The remaining documents are available in iPortal > Publication Zone.